Other Parts Discussed in Thread: SN74HCS573, SN74LVT573, SN74AHC573
Tool/software:
When converting from 5V to 3V using the standard logic IC573, which of the SN74LV573, SN74LVC573, SN74LVT573, or SN74HCS573 is best to choose?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
When converting from 5V to 3V using the standard logic IC573, which of the SN74LV573, SN74LVC573, SN74LVT573, or SN74HCS573 is best to choose?
The HCS device does not have overvoltage-tolerant inputs and cannot do this.
The main difference between the AHC (SN74AHC573), LV-A, LVC, and LVT devices is the output drive strength (4 mA, 8 mA, 24 mA, 32 mA); to reduce EMI problems, choose the smallest one that is sufficient for your application.