This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC2G07: Schematic verification

Part Number: SN74LVC2G07

Dear Team,

Need you to verify the schematics and clear a few doubts.
The fan i am using has a internal PU in the PWM signal and is PU to 5V as below attached image.
So the buffer input is 1.8V from PS FPGA and output will be 1.8 right? 
So can the PWM directly connected to the PWM which is internally PU and connected to 5V input

image.png

Regards,
Irfan

DESIGN8.pdf