Hi,
Our customer would know VT+Max VT-Min for reference at VCC=1.1V/1.4V and temperature= 0~75℃.
Because customer's system should be VT+<0.84V and VT->0.36V.
Can I receive these data/temperature=0~75℃
Best Regards,
Kato
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Our customer would know VT+Max VT-Min for reference at VCC=1.1V/1.4V and temperature= 0~75℃.
Because customer's system should be VT+<0.84V and VT->0.36V.
Can I receive these data/temperature=0~75℃
Best Regards,
Kato
Hi Kato
I have attached the data I have. as you can see they do not meet spec even at 25deg shown highlighted.
I also checked AUP1G17 and it can not work with their levels.