I am using the AND gate SN74LV08A and 1Y was exposed to 11.5V while VCC was 3.3V. Could this harm the chip in any way?
Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Currently we are seeing an offset on the output 1Y When the inputs of the gate are 0 as shown below. Do you have any suggestions how we can get the output as close to 0 as possible?
Would a pull down resistor help lower the voltage to less than .5V? Thanks
Vcc = 3.3V
IN:1A 3.3V
IN:1B 0V
OUT:1Y 1.6V
IN:1A 3.3V
IN:1B 3.3V
OUT:1Y 3.3V