This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

a question about SN74LVCH16T245DGVR

Other Parts Discussed in Thread: SN74LVC16T245

Hello,

Do I need series termination resistors on the signal lines interfacing with 1.5 ft cable so that oscillation or ringing can be prevented?  The power supply of the device is 5V for my application.

Thank you,

  • The SN74LVC16T245 does not integrate series resistors, so if necessary there should be external series resistors to minimize signal overshoot and undershoot.

    This app note also has additional information about termination options. Pages 20 to 22 goes into detail of possible output termination options, and when they should/should not be implemented.

    Best Regards,
    Nirav