Hello
What is the difference SN74HC244 and SN74AHC244? thanks
Regards,
Nanfang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
What is the difference SN74HC244 and SN74AHC244? thanks
Regards,
Nanfang
SCAA034: AHC Logic Family says:
Some advantages of using AHC over HC are:
- The AHC logic family is almost three times faster than the HC family. The AHC logic family has a typical propagation delay of about 5.2 ns.
- The AHC logic family allows designers to combine the low-noise characteristics of HCMOS devices with today’s performance levels without the overshoot/undershoot problems typical of higher-drive devices.
- The AHC family has lower power consumption than the HC family.
- The output drive is ±8 mA at 5-V VCC and ±4 mA at 3.3-V VCC.
- …