Hi,
I'm using TI's SN74LVTH574, and connect unused input and output pins to ground.
However give signal to OE, SN74LVTH574 do not operate.
So let input to ground, and make output to floating, then operate normally.
when output is connected to GND, the power is switching as if the 3.3V is go through to ground.
I'd like to know the reason of this situation.
at SN74LVTH574 datasheet, there is explanation only for unused input pins.
And I can't find any comment for unused output pins.