Hi,
I want to interface two TTL IC's,in that assume one is working at 3,3V and the other is working at 5V.
Do I need to use a voltage level translator IC?. If yes why if no why.Please reply.
Thanks&Regards
Hari T O
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TTL always means 5 V. There is a standard called LVTTL for 3.3 V devices, which uses exactly the same thresholds as TTL.
Some people mistakenly use "TTL" to describe CMOS ICs, which can be incompatible with actual TTL ICs at the same supply voltage.
So unfortunately the word "TTL" contains no information at all. Specify the exact IC model, and its properties, and in which direction the signals go in your circuit.