Hi all
Would you mind if we ask SN74AUP3G14?
On the data sheet, Recommended Low-level output current in case of Vcc=3V is 4mA.
Our customer use 6mA(IOL) with Vcc=3.3V.
So, might it cause of thermal problem?
Kind regards,
Hirotaka Matsumoto
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
Would you mind if we ask SN74AUP3G14?
On the data sheet, Recommended Low-level output current in case of Vcc=3V is 4mA.
Our customer use 6mA(IOL) with Vcc=3.3V.
So, might it cause of thermal problem?
Kind regards,
Hirotaka Matsumoto
When you overload the output, the voltage drop becomes larger. So in the worst case, you get a voltage drop somewhat larger than the specified 0.45 V at 4 mA. (And in the typical case, you probably won't even go above 0.45 V).
Anyway, even with a completely unrealistic voltage drop of 3 V on all three outputs, the power dissipation would be 3 × 3 V × 6 mA = 54 mW. In the DQE package, this would result in a temperature increase of 54 mW × 261 °C/W = 14.1 °C, which would be completely harmless.