Other Parts Discussed in Thread: ISO7640FM
Hi,
I'm developing with SN74LVCH16T245 right now, to transfer 3.3V from/into 5V in my design, but I found the signals are interfered by the following circuits, so I want to replace it with an isolated one, which has the same characteristics with this one, but plus isolation feature, they are:
- 3.3V into/from 5V
- 16 channels
- maximum 4.3ns of propagation delay or lless, the less the better
- isolated between input and output
please give me some recommendation, thanks a lot!
Best Regards,
Bruce