Part Number: TXS0108E
Hi,
the TXS0108 was used to translate the level from 3.3v to 5v on the SPI_CLK signal. The CPU is STM32F427 and the output was set to PUSHPULL.
i found that the input of the TXS0108 is right, but the output was wrong,even i try all of the follow method:
1.change the RP7 from 33R to 0R
2.remove the RP2 so the TXS is isolated with the SPI device
3.remove the RP7 then input another SPI-CLK from a normal development board(the cpu is stm32f401)