Part Number: SN74AVC8T245
Other Parts Discussed in Thread: ASH
Hi,
I am using SN74AVC8T245RHLR part in my board.Previously there was requirement of data transmission is in only one direction so I was making DIR pin low and signal is going from B port to A Port.
But now new requirement came in which data should flow in both the direction, so for this I tied the DIR pin to one of GPIO pin. When I set GPIO as LOW then data transmission is from B to A.
And if I set the GPIO pin as HIGH then the direction should be A to B but I am not able to read proper output.
I have one doubt that Can i toggle the DIR pin of level translator when the enable pin is LOW(active state) or first I need to put the enable pin as tristate and then I need to toggle the direction and then I need to
make enable as low again.
Thanks
Ash