Part Number: LSF0108
Other Parts Discussed in Thread: LSF0101
Hi team,
My customer wants to use LSF0108 IBIS model to do some simulation. Here're some questions:
1. They're using LSF0101_IO_33_S model to do the behavior level simulation. Is that correct?
2. Use-case is 1.8V VDD1 and 3.3V VDD2. If customer use 50Ohm pull-up on B output, they found the A input will also be pulled up to ~2V. What do you think might cause this problem?
Thank you!