Other Parts Discussed in Thread: SN74LVC8T245, SN74LVC2T45, SN74LV1T34, SN74AHCT1G125, SN74LVC1T45
Hello Community,
We need to interface a TM4C (3V3) SPI bus into a sensor that requires 5V digital input.
The design currently uses SN74LVC3G34DCTR, and it DOES work. However, when reviewing the datasheet, I noted that the minimum logic high level is 0.7*VCC, which is 3.5V, when we are actually only sending 3V3.
In order to avoid producing the boards with that "known irregularity", we would like to know if there a TTL alternative to that part?
Regards
Bruno