Other Parts Discussed in Thread: SN74LS09,
In an existing application, I’m trying to replace an SN74LS09 which currently interfaces with 5V logic to a part that will interface with new 3.3V logic. Ideally, I would like to do it with a drop-in replacement, but if that is not possible then to do something else with as few parts as possible.
The one option that I’m looking at is to use an open-drain SN74AHC1G09 operated from a supply of 3.3V, but I have question on the rating of the maximum output voltage. I’m trying to figure out if the output is diode clamped to Vcc or not. It seems to indicate that it is, but I want to make sure. Also, it seems odd to me to have an open-drain output clamped to Vcc, but maybe that is normal.
If I have a resistor pullup of 1.5 kΩ to 15V on the output of the SN74AHC1G09;
1) What will the output voltage be when it is a high output.
- 15V? OR,
- 4V because it is diode clamped to the supply of 3.3V?
i. Current is limited to about 7.3 mA which is less than the absolute maximum of 20 mA.
2) Was the output of the SN74LS09 also clamped to Vcc or not?
From the data sheet:
Absolute Ratings
(2) The input and output voltage ratings may be exceeded if the input and output current ratings are observed.
Thanks for any help you can provide.