Other Parts Discussed in Thread: SN65LVDS301
Hello team,
my customer is asking for the decoupling caps of the SN74LVC16244. As it has 4 supply pins, the recoommendation is:
"For devices with a single supply, 0.1uF is recommended. If there are multiple VCC pins, then 0.01 or 0.022uF is recommended for each power pin. It is acceptable to parallel multiple bypass caps to reject different frequencies of noise. A 0.1uF and a 1uF are commonly used in parallel.
In my opinion, the statement is not clear, as all LVC16244 have in total 4 supply pins. What is the recommendation? Use at each pin 0.01u to 0.022u cap and then paralell them with 0.1uF each?
Another point is the rise and fall times of the device. The LVC16244 is driving the input pins of the SN65LVDS301, with an input capacitance of 1.5pF. Do you have a quick estimate of the rise and fall times?
Thank you very much and kind regards,
Felix