Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AUP1G79: How to use this part on downclocking application? 5kHz to 2.5kHz.

Part Number: SN74AUP1G79
Other Parts Discussed in Thread: SN74AUP1G80,

Hi Team,

How to use this part on downclocking application. 5kHz to 2.5kHz?

5kHz input to pinD?

How to set CLK signal?

Thanks

  • Hi Daniel,
    The SN74AUP1G79 is not ideal to use as a clock divider since it does not have an inverted output. I would recommend using the SN74AUP1G80 instead. If you are set on using the 1G79, just add an inverter after Q to get Q\ and use the diagram from the 1G80 datasheet.

    The datasheet includes an application for exactly what you are wanting to do on page 10.