This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0104: SPI lines voltage level translator

Part Number: TXB0104

Hi,

Can I use this "TXB0104" for 1.2V to 1.8V SPI lines level translator. With speed upto 16Mbps ?

  • The datasheet guarantees 20 Mbps (see tables 6.6 and 6.11), if your drivers are string enough, and the parasitic capacitances of your circuit are small enough.

    SPI signals are unidirectional, so unidirectional or direction-controlled translators would be more robust. Why do you want to use an auto-direction-sensing translator?