Other Parts Discussed in Thread: TINA-TI
Hello I was wondering the following,
if the SN74LS249 Inverted Flipflop can drive a 50Ohm bnc cable which is terminated on the other side with 10K.
which bnc driver should I include if not?
the sn74ls279a is it used for 5V or 7V?
Best
Bastiaan