Hi,
I am using SN74LVCH16T245DGVR in one of my project. Here I am driving 16 IO's from A port ofSN74LVCHT245DGVR.pdf to B port of SN74LVCH16T245DGVR. Here A port is referenced to 1.8V and B port is referenced to 3.3V.
When I am driving logic high(1.8V) from A port to B port of SN74LVCH16T245DGVR, When I probe at B port on those particular pins I am getting around (1.2V) where I should get (3.3V) as logic high on those pins. And also when I am driving logic low (0V) from A port to B port of SN74LVCH16T245DGVR, when I probe at B port those particular pins once again I am getting around (1.2V) where I should get (0V) as logic low What should be the cause for voltage dipping?
Hereby I am attaching the schematics of SN74LVCH16T245DGVR for your reference.