This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN7407: SN7407 Cascade Buffer Driving

Part Number: SN7407


if i do use the same buffer and use two internal buffers to drive the same signal its ok to connect the first and second driver without the need of a pullup resistor.

what i wanted to do is to buffer a signal coming from a low current source, then this signal will drive some relay and LED's then I’m driving this signal after the first buffer to 3 more buffers on the same package.

is like having one signal going to a first buffer, then a second buffer and from the second buffer to 3 buffers is parallel, and mi question is from buffer one to buffer one is a pull up needed?

Best Regards

Ulisses