This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC04A: How is the spec 'tsk(o)' defined?

Part Number: SN74LVC04A


Hi team,

There is a spec, tsk(o), in SN74LVC04A datasheet. As my memory there is two kinds of output skew spec definition for logic device: one is channel to channel output skew, another one is the difference between low-high and high-low edge propagation delay (tPLH-tPHL). I am wondering which kind of skew tsk(o) is specified for SN74LVC04A?

Thanks,

John

  • Hi John,

    In short - the first one.

    The answer you're looking for is available in the application report Understanding and Interpreting Standard-Logic Data Sheets on page 53:

    4.9.16  tsk(o) Output Skew

    JEDEC - The skew time between two outputs of a single integrated circuit with all driving inputs switching simultaneously and the outputs switching in the same direction while driving identical loads.

    TI - The skew between specified outputs of a single logic device, with all driving inputs connected together and the outputs switching in the same direction while driving identical specified loads.