This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC244A: high speed signal

Other Parts Discussed in Thread: SN74LVC244A

Hi,

Customer of mine is using SN74LVC244A for video signal buffer.
As the video camera is high resolution, the clock frequency is likely to be 70 MHz or higher.

May I if this device can operate normally when signal is around 70Mhz?
Including the propagation delay as well. The Vcc is 3.3V

Thanks