Other Parts Discussed in Thread: SN74CBTLV3257, TS3A5018, TMUX1574, SN3257-Q1, SN74AXC4T774
Hello
I use the TXS0104E to translate voltage for a Quad-SPI bus from MCU STM32F777 run at 3.0V (VCCB) to a 2:1 MUX P/N SN74CBTLV3257 run at 1.8V (VCCA) (*). The MUX output is connected to a 1.8V Micron flash. The voltage translator is used as is without external pull resistor.
We run on a clock ~ 16.7 Mhz. I notice that the output signal amplitude of the TXS0104E reaches 1.8V at the beginning of the signal for a very short time and then drops quickly to stabilize around 1.5V. That observation is for SPI bus data outputs. For clock signal, its amplitude is constant around 1.6V. Input signals are clean transitions between 0V and 3V.
Question: why can the amplitude not reaching and stabilizing at 1.8V?
(*) the MUX is specified for 2.3V to 3.6V operation, I assume running it at 1.8V would incur higher Ron and slower switching time but since we do not MUX the Quad SPI bus in real time but only occasionally between MCU and FPGA so it should not matter much