Part Number: TXB0102
Other Parts Discussed in Thread: SN74AVC2T245, SN74AVC4T245
Hi team,
My customer is using this device to realize voltage level translator for UART between MCU and slave device. VCCA=1V8, VCCB=3V3, and they find that when A1=0V, B1 will about 1.5V, this will cause data error in this application. We suspect that this is because we have internal resistor 4kOhm in the output, when customer have pull up resistor (4.7k for example) in the B side, this will cause B1 still have about 1.8V when A1=0. We may need team's help below,
- Is the internal resistor cause this issue? Why we have this resistor?
- Is it possible if we use B1/B2 to send the data as well as driving LED load?