Part Number: SN74123
Other Parts Discussed in Thread: SN74LVC1G123, CD74HC221, TS5A3160
This is in reference to the output obtained from the SN74123 (https://www.ti.com/lit/ds/symlink/sn74123.pdf), I want to change the output voltage from the usual +5V pulses. Do I have to change the input to Vcc and CLR pins (pins 16 and 3 respectively)?
If I want to obtain discrete outputs of +1, +2, +3 and +4V how would I be able to?
I wasn't able to find any direct mention about varying output in the Designing with Monostable Multivibrators booklet (http://www.ti.com/lit/an/slva720/slva720.pdf)
Any help is greatly appreciated