We used IC under the following conditions.
Why does this IC drop voltage?
I thought I would do vCC level OUTPUT. Can you explain the mechanism?
Input : 1.8V
VCC :3.36V
output:約3.12V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We used IC under the following conditions.
Why does this IC drop voltage?
I thought I would do vCC level OUTPUT. Can you explain the mechanism?
Input : 1.8V
VCC :3.36V
output:約3.12V
Thanks you for your quick reply.
i have a question.
We need ICC around 2mA or 4mA.
How many volts do you guess VOUT will be under these conditions?
Best Regards, BANE
The worst-case voltage drop would be 90 Ω × 2 mA = 0.18 V or 90 Ω × 4 mA = 0.36 V. (The typcial voltage drop is smaller.)