This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74F157A: ESD Ratings

Part Number: SN74F157A

Hi,

I need the ESD ratings for the SN74F157AD.   

Thank you,

HSG 

  • Hello HSG,

    I don't currently have a test report for this device, so I would have to list it as "minimal ESD protection" - which puts it in ESD Class 1 ≤1999V HBM

    We currently have a relatively large backlog of devices that need ESD testing, so it will be quite some time before I can get results for you. Please contact me directly by email if you need the results urgently and we can work to prioritize accordingly.

  • Hey HSG,

    As per my email, I wanted to provide an update for this post.

    I was able to find a report that showed that this device is rated for:

    HBM: 3kV

    MM: 300V