Part Number: TXB0108
Other Parts Discussed in Thread: SN74AHCT541
Hi,
can I use TXB0108 as unidirectional level translator from 3.3V to 5V
Warm regards,
Monisha om
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TXB0108
Other Parts Discussed in Thread: SN74AHCT541
Hi,
can I use TXB0108 as unidirectional level translator from 3.3V to 5V
Warm regards,
Monisha om
The load restriction applies only to the data I/Os. The OE pin is a high-impedance CMOS input and works with any pull-down value.
To convert unidirectional 3.3 V signals to 5 V, you do not need an auto-bidirectional translator; you could just as well use a buffer with TTL-compatible inputs like the SN74AHCT541.
Thanks for your response .
Already layout everything complete with this TXB0108 IC. So may I know If I use TXB0108 for unidirectional, is there any issues?
Warm regards,
Monisha OM
See the datasheet. The TXB output drivers are very weak, and the edge accelerators can be falsely triggered by ringing on the signal lines, so you cannot use long traces.
Hey Monisha,
Since this device will be translating between two MCUs (high impedance inputs), then there will likely be no issues. As Clemens' has stated, long traces will add more capacitive loading so its recommended to keep them short to avoid the issues that were also highlighted by Clemens.