Other Parts Discussed in Thread: SN74AUP1T08, SN74AUP1T57, SN74LV1T08, TXS0101, TXS0102-Q1
hi, Pls help suggest a single/dual non-inverting buffer as below spec
VCC:3.3V
input: Vih>1.35V, Vil<0.45V
output: Voh>2V, Vol<0.8V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SN74AUP1T08, SN74AUP1T57, SN74LV1T08, TXS0101, TXS0102-Q1
hi, Pls help suggest a single/dual non-inverting buffer as below spec
VCC:3.3V
input: Vih>1.35V, Vil<0.45V
output: Voh>2V, Vol<0.8V
Hey Jazz,
Those input thresholds are low, we wont have a device to support this.
These input thresholds require voltage-shifting gates in the LV1T or AUP1T families. There is no single-input buffer, but you can use AND, OR, or configurable gates: SN74LV1T08/32, SN74AUP1T08/32, SN74AUP1T57/58/97/98/157/158.
The output voltages depend on the output current.
hi ,
Thanks!
Pls suggest a single port level shift with EN function such as TXS series and meet AECQ spec. For TXS0101, do we have part number with AECQ?
Hi Jazz,
We do not offer single port auto bidirectional translation with automotive qualifications. We do offer a dual channel TXS0102-Q1 translator which is rated for automotive spec.
If you have any more questions about new topics, please post them to their own threads.
Thanks!
Chad Crosby