Part Number: SN74LVC541A
Dear team,
Customer tested that when the voltage of Pin 6 >5.5V, this channel will be hurt and the output always low. I see from datasheet that the absolute voltage of Pin 6 should be 6.5V. And the fault rate is about 4/226=1.7%, and always pin 6 faults, other IOs are normal.
Would you kindly help confirm the absolute voltage?
Thanks.
Best regards,
Sammi