Other Parts Discussed in Thread: SN74AUP1G08, SN74AUP1G34
Dear Support team,
Logic devices SN74AUP1G14, SN74AUP1G34 and SN74AUP1G08 datasheets specifies the Operating free-air temperature range (TA) from -40 to 85°C whereas Tjmax allowed is 150°C. If we have a scenario wherein ambient air temperature is > 95°C but still IC junction temperature, Tj <= 130°C is this ok? Will these logic devices behave or have same electical characteristics as specified in this case?
Thanking you in advance.