Part Number: LSF0204D
Other Parts Discussed in Thread: LSF0204, TMUX1574, SN74AXC4T774
Hi Texas:
We would like to know the propagation delay of LSF0204DRUTR
I also checked the former issue page "LSF0204: Propagation delay of LSF0204RUTR"
You said that the load capacitance and resistance and any pullup resistor will impact the propagation delay
Because our SPI topology Tclk frequency is 66MHz and the delay time budget of level shift element need to be 1ns or at least below 1.5ns
From VDD 1.8V to VDD 3.3V, our P3V3 pullup resistor is 10K and no load capacitance and resistance
Can this level shift meet time delay requirement?
Thanks
Nick