HI,
In my design, am using SN74LVC8T245. VCCA is connected to 3.3V, VCCB is connected to 5V and DIR, OE pin are connected GND.
We are converting 5V to 3.3V logic. The signals are connected to the connector. The issue is 5V logic input signal level is not going to 5V(I am getting 1.5V).
If disconnect 245, the input signal is reaching to 5V. I have checked the following things in the circuit.
1) Cin and Cout are matching.
2) no short circuit on the board.
Please help me out. How to solve this issues.
Thanks,
Sankar.K