Other Parts Discussed in Thread: SN74LVC8T245
I'm using a SN74LVC8T245 in an embedded application and am seeing a 0.8ms output pulse when the input is low and the input power is ramping from 0-3.3V. The output rail is 5V and is up approximately 2.2ms prior to this event. The 3.3V bus is around 0.8V-1.2V when this occurs and it is ramping at a rate of 0.5V/ms.
My intent is to have this output be high impedance until both rails have powered up and the DSP chips driving them have gone through configuration steps.
Unfortunately, this high output occurs even when the output enable (!OE) is pulled up to 3.3V by the input voltage on either side. I originally had the Output Enable connected via pull-up resistor to the 3.3V rail when I first encountered this issue. Suspecting it needed a firmer voltage, I connected it via a 3.3V/5V (10k and 20k) voltage divider to the 5V supply. It still occurs in exactly the same manner on all channels.
I'm confused because this output should not be occurring per the notation in the datasheet at http://focus.ti.com/lit/ds/symlink/sn74lvc8t245.pdf page 2:
"To ensure the high-impedance state during power up or power down, OE should be tied to VCC through a pullup
resistor; the minimum value of the resistor is determined by the current-sinking capability of the driver."
Has anyone else encountered this discrepancy or is the chip suspect?
Thanks.