This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello everyone,
I have 3 I/O 5V TTL bidirectionnal (each signal have one input, one output and one output enable).
In my previous systems, I used this component SN74LVT244B (with 74AHC1G125GW) to have bidirectionnal translation between 5V TTL from/to 3.3V LVTTL.
Now, I want to connect these 3 5V signals to my Virtex 7 evaluation board.
The problem is that the Virtex 7 only accepts LVCMOS 1.8V. Which component do you advice me to take?
Should I keep the SN74LVT244B ((with 74AHC1G125GW) to convert to 3.3V LVTTL and then use another component to translate to LVCMOS 1.8V ?
Thanks for your answers and happy new year,
Thibault
Hello,
Thanks for your quick answer :)
I did a quick schematic of my system. Hope this can help you understand my need and precise me what option I should go for.
I've got 3 wires (from a dsub connector) that are dividing into 9 channels (the input and the 2 output for the 3 wires). These 9 channels are connected to a FPGA board (here Artix 7) via a cable.
I've got another concern that is related to the distance max for lvcmos signals.
Indeed, I want to make the adaptation for my signals on my board and connect all my lvcmos signals directy to my FPGA board via a vhdci cable (approximately 1 meter)
Thanks
Hello,
No my wire on the left is not a bus.
How should I proceed then to have an input or an output (controlled by OE) on a single wire with SN74LVC1T ?
Knowing that my 3 right signals are 1.8V voltage and my left signal is 5V.
Thanks