Part Number: SN74LVC244A
Other Parts Discussed in Thread: SN74AUCH244, SN74AUC244, TXS0108E, LSF0108
Hi Sir,
We are looking for MDIO/MDC buffer and operation in 1.2V, SN74LVC244A can meet the request but can't operation in 1.2V,
Could you please help to recommend which part is suitable for the application?
Below is the additional requirement from customer.
How about SN74AUCH244? please advise.
Thanks
1. Open drain buffer is not recommended for MDC
2. MDC/MDIO skew caused by the propagation delay should also be examined.