Part Number: LSF0108
Hi Sir,
My customer found the LSF0108 slew rate is too slow as below diagram CH1(CLK).
And also insert the schematic, FYI
Could you please help to comments how could we fix it?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LSF0108
Hi Sir,
My customer found the LSF0108 slew rate is too slow as below diagram CH1(CLK).
And also insert the schematic, FYI
Could you please help to comments how could we fix it?
Thanks
The application report Voltage-Level Translation With the LSF Family (SLVA675) says:
5.4 What is the frequency range of the LSF?
The LSF family can translate up at 100 MHz and down at 200 MHz with reasonably good signal integrity. Signal integrity for translation depends on many factors, including line capacitance, output load, and pullup resistor sizes. Generally, smaller pullup resistors allow faster translation, but at the expense of power.
Those 10 kΩ resistors are certainly too large. Depending on the frequency, you might also want to reduce the pull-ups on the B side.
Hi Anne,
There is no max as such for this device as compared to TXB/TXS.
The Cload is referencing to the output and with smaller loading, higher Rpullup can be used or theoretically can achieve higher speeds at the expense of power consumption.