Part Number: SN74HC595
Hello,
I want to know if 12.5 MHz can be supported on SN74HC595 when Vcc=3.3V under 85 degree ambient temperature.
Could you help? thanks!
Regards,
Tony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN74HC595
Hello,
I want to know if 12.5 MHz can be supported on SN74HC595 when Vcc=3.3V under 85 degree ambient temperature.
Could you help? thanks!
Regards,
Tony
Hi Tony,
The max frequency range listed in the datasheet is of 2V 5MHz, 4.5V 25MHz, 6V 29MHz. These values are guaranteed and measured at a 50pF load over the entire operating temperature range including 85C.
So assuming a linear relation between voltage and frequency and using the two external points of 6V and 2V, we see that at 3.3V, the device should have a max frequency of 12.8MHz. The actual max frequency should be higher than this because the relation is not linear but more logarithmic. However if your load is higher than 50pF, then your max frequency might be a bit lower.
I would say if your load is less than 50pF, the device should support 12.5MHz at 85C at 3.3V Vcc.
Thanks!
-Karan