This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Is the reliability of a logic device affected by applying an input voltage larger than the supply (VCC)?



FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ

The reliability of a logic device is linked to the recommended operating conditions in the datasheet. As long as the device is operated within the recommended operating conditions, the reliability data provided for the device is valid.

If, for example, a device has a recommended maximum input voltage of 5.5V, and an absolute maximum input voltage of 6.5V, then reliability would only be guaranteed up to 5.5V, and reliability could be reduced with an input voltage between 5.5V and 6.5V.  Beyond 6.5V the device could fail immediately.

See also: [FAQ] How do I find reliability data for a logic device?