Dear,
I know the max input overshoot & undershoot value will be the absolute max/min rating of Vcc in the datasheet, and TI don't guarantee any operation outside this range.
But my customer would like to know the actual value of input overshoot & undershoot of SN74LVC3G17 and if it is possible to operate in the conditions as shown in the pictures.
I've learned from another e2e article, that logic which without clamp diode, the input overshoot under 1.3Vcc(=8.45V[6.5*1.3]) is acceptable(Actual Value).
And also the input undershoot under Vpeak-1(=-1.5V[-0.5-1]) within 10ns is acceptable(Actual Value).
According to above, I think overshoot (pic1, Vmax=6.8V) will be no problem.
But the undershoot(pic2, Vmin=-840mV, lasts 200ns) may cause the problem(because the period is too long).
And what can be concerned if the overshoot & undershoot occurs 1000 times/sec?
Please let me know if I got anything wrong.