Part Number: TXS0108E
Other Parts Discussed in Thread: SN74LVC8T245, , SN74AHCT541
Hello,
I'm having issues with this chip after connecting output signals are connected to the load.
This is the schematic:
This is one of the output signals (no load). The frequency is the same as the square input signal and the voltage level is 5 V as expected. Not sure why it has this small voltage drop of 300 mV.
Then when I connect the load with a 15k input impedance. This is the signal observed.
The square wave is completely distorted. The frequency is over 38 MHz.