Part Number: SN74AXC8T245
Team,
Using the SN74AXC8T245 in a design and I am curious what the maximum current drive is on an output pin. The datasheet shows an absolute max of +/-50 mA and then farther down there is a test with a 2k Ohm load resistor but is there a recommended maximum current that this part can drive?
Also I just realized that the vendor that made the board for the customer tied DIR1, DIR2 and OE_N directly to GND or VCC. The application circuit shows that these are usually pulled up or down with 10k resistors. Any issues with these direct ties to power or GND? It doesn’t sit great with me but we don’t see crazy increases in current when we apply power to this part of the board.