Part Number: SN74AUP1G57
Other Parts Discussed in Thread: SN74AUP1G97, SN74AUP1G98, , SN74AUP1G58
Hi,
I am referring to the following “Low Power Configurable Multiple-Function” gates:
a) SN74AUP1G97
b) SN74AUP1G98
c) SN74AUP1G57
d) SN74AUP1G58
The datasheets do not provide any minimum value for the input voltage slew rate. They basically state that the Schmitt-trigger inputs will allow for slow signals at the input. I am designing circuitry for an energy harvesting application where some of the signals may take anywhere from 5 minutes to 30 minutes to ramp from ground to the desired voltage at which switching should occur. Can the Schmitt-trigger inputs in the above part numbers accommodate the inputs I am talking about?
Thank you!