Other Parts Discussed in Thread: SN74LS47
Hi all!!
I am using SN74LS47 to connect 12 seven segment displays to LM4F232H5QD MCU, I am planning to use BCD to SEVEN SEGMENT DIVIDER SN74LS47. As per the datasheet 46A, 47A and LS47 will be used for common anode seven segment displays. But same series has got 3 blanking and LT pins, Can I short all these three pins of all SN74LS47 all together for all 12 drivers? My intention is to display DD.MM.YY and HH.MM.SS
Thanks and Regards
-Anand