This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Quickswitch / Level Shifter for modern FPGAs



Hi all,

Modern FPGAs are so cool. So much logic in such smal packages.

But the io-voltage they can deal with is limited to 3.3V or less, and undershoots have to be limited to less than -0.5V.

I am looking for a level shifter technology that allows me to connect 5V signals on one side, and a modern FPGA on the other side. This level shifter should:

  • bidirectional without direction signal
  • limit the output high voltage to its own supply voltage
  • limit undershoots to less than -0.5V
  • limit overshoots to less than vcc+5%

Does anybody know a suitable device from TI?

Regards,

Niels

  • Hi Niels

    The CB3T family of devices will translate a high voltage to the supply voltage. The requirement is that the input voltage be 1V above the supply voltage.  Here is an example. SN74CB3T3245 They are switches so they dont need a direction pin.

    When going back the other direction. Low to High you will need a pullup to get the signal back up to 5V.

    I also attached an appnote with a brief explanation.

    They aslo use voltage clamp type devices in this situation. Here is an example of that SN74TVC3306.

    You can find appnotes on this type of part in the product folder on the web..  This forum olny allows me to attach one item.

    CBT-C CB3T CB3Q.pdf
  • Hi Chris,

    well, we tried CB3T, but failed. The Problem is, that the 5V-side is a bus that is sometimes driven with 3.3V Signals. Pullups on the 5V side are not allowed.

    An example would be if I want to add a 3.3V device to a PCI-Bus that contains 5V devices.

    If the 3.3V device drives a signal (with 3.3V high level), the CB3T limits the voltage on the "bus" side to 2.3V or less, depending on the current drawn by the other devices on the bus. This is not practicable in this case.

    What I am looking for is a signal switch that lets pass all voltages between GND and its own supply voltage. All voltages above its power supply and below ground shall be blocked.

    Maximum input voltage shall be >5Volt.

    This would be a really great device for many kinds of applications with modern FPGAs.

    Regards,

    Niels

  • You should be able to use a voltage clamp type part. This would pass voltages up to Vref. The issue is you would need the part powered by a voltage 1V greater than Vref. So if you could power the part with 5V and set Vref to 3.3V then the signals going through the switch would be clamped at 3.3V in either direction.

    The SN74TVC3010 is an example.  we also have some new parts about to be released.

    I attahced an slide show that has some explination of how they work.

     here is my Email if you need more info. c-cockrill@ti.com

    voltage clamps( Alvin).pptx
  • Hi Chris,

    I had a look into the TVC documents, and I worry about two points:

    (1) the propagation delay is 0-4ns. this is a large spreading and 4ns is too much for e.g. PCI.

    (2) what about undershoot clamping? Modern FPGAs accept negative input voltages up to -0.5V and voltage below this may hurt the FPGA.

    Thanks in advance,

    Niels

  • Hello Chris and the rest of the comunity,

    is there any chance for a solution that allows to connect modern FPGAs to a mixed 3.3V / 5V environment like e.g. a PCI-Bus?

    Regards,

    Niels