Other Parts Discussed in Thread: MAX232, SN74LVC1G34, SN74AHC1G125
Hello, I am needing help selecting level translator for a project. I want to take the output signal (TX) from a MAX232 chip and input the signal to my FPGA (Xilinx KC705 eval brd). It is my understanding that the output of the MAX232 chip is 5V TTL logic. I do not believe that my FPGA pins support 5V TTL. I have seen different types of level shifter (voltage and mixed signal). I want to target IOSTANDARD LVTTL or LVCMOS on the FPGA pin. It is my understanding that if I use LVTTL/LVCMOS standard then my input signal needs to comply with LVTTL/LVCMOS standard. I feel like I need a level shifter that will convert from 5V TTL to 3.3V TTL ( which I believe is LVTTL). Could help me gain a better understanding on how to select the correct product? Thank you for your time.
Adam