Part Number: SN74LVC2G74
Other Parts Discussed in Thread: SN74LVC2G17
Hello,
I have an electronic board to make, those functions are :
- make acquisitions of two TTL signals (motor encoder output, max frequency is around 70kHz)
- divide by 4 the frequency of these two TTL signals
- shift the level voltage from TTL to 24V (will be plugged to logical inputs of an ECU)
For acquisition and frequency division, I plan to use a SN74LVC2G17 (schitt-trigger buffer) followed by two SN74LVC2G74 (D-type flip-flop) in serie.
Then, for the voltage level translator from 5V to 24V, I am not sure which component to use ... I was thinking using an opto-isolator like the ACPL-M43T (as I didn't find any TI isolator that allows 24V) but not sure it is a good solution.
Which component would you recommend to make the voltage level translator 5V (TTL) --> 24V ?
Thanks,
Best regards,
Julien