Part Number: TXB0104-Q1
Hi,
I am Using the TXB0104-Q1 device for VCCA = 3.3V and VCCB= 5V. I am trying to calculate the power dissipation of the device. In the datasheet the parameter " Power Dissipation Capacitance" CpdA and CpdB are given.
Should the Static Power be calculated seperately for VCCA and VCCB?
I do not have any external load capacitance connected in my design.
What is that external load capacitance used for?
What is the maximum Power dissipation rated?
Regards
Gayathri