Hello all,
I always like it when a datasheet provides layout hints.
For the SN74LVC2G14, the datasheet shows the following layout example:
I assume that the 0.1 µF capacitor is meant to operate as a bypass capacitor to prevent power disturbances. However, I think this layout doesn't work as expected. What is Vdd?
I believe that the capacitor should be placed below the IC and connected to pin 2/3 and pin 5. Or am I missing something?
Thanks.
Daniel